These bits select the input source for generating the CRC, as shown in the table
below. The selected source is locked until either the CRC generation is completed or
the CRC module is disabled. This means the CRCSRC cannot be modified when the CRC
operation is ongoing. The lock is signaled by the CRCBUSY Status bit. CRC generation
complete is generated and signaled from the selected source when used with the DMA
channel.
| Value | Name | Description |
|---|
| 0x00 |
NOACT |
No action |
| 0x01 |
IO |
I/O interface |
| 0x02-0x1F |
- |
Reserved |
| 0x20 |
CHN0 |
DMA channel 0 |
| 0x21 |
CHN1 |
DMA channel 1 |
| 0x22 |
CHN2 |
DMA channel 2 |
| 0x23 |
CHN3 |
DMA channel 3 |
| 0x24 |
CHN4 |
DMA channel 4 |
| 0x25 |
CHN5 |
DMA channel 5 |
| 0x26 |
CHN6 |
DMA channel 6 |
| 0x27 |
CHN7 |
DMA channel 7 |
| 0x28 |
CHN8 |
DMA Channel 8 |
| 0x29 |
CHN9 |
DMA Channel 9 |
| 0x2A |
CHN10 |
DMA Channel 10 |
| 0x2B |
CHN11 |
DMA Channel 11 |
| 0x2C |
CHN12 |
DMA Channel 12 |
| 0x2D |
CHN13 |
DMA Channel 13 |
| 0x2E |
CHN14 |
DMA Channel 14 |
| 0x2F |
CHN15 |
DMA Channel 15 |