2.5.2.4 Valid Code Detection in Secure Boot Mode
The valid code detection in Secure Boot mode is similar to the one in Standard Boot mode. However, additional checks and operations are performed.
If the initialization of NVM is successful, the ROM code reads and deciphers the first 32 bytes of the potential secure boot file to find a valid Arm exception vector table (see Arm Exception Vectors Check). From the sixth vector, the ROM code extracts the size of the boot file including its signature. When the AUTH_MODE field is set to 1 in the Secure Boot Configuration Packet, the size of the X.509 certificate chain is also extracted. The boot file size must be 16 bytes aligned (AES block size). The sum of the boot file size and the certificate chain size must be lower than the maximum bootstrap size. If these first validations fail, the ROM code restores the memory interface PIO and its settings to their reset values and then tries to boot on the next NVM in the boot sequence.
Otherwise, the total size is used to copy the boot file, its signature and the X.509 certificate chain from the NVM into the internal SRAM.
Next, depending on the AUTH_MODE field in the Secure Boot Configuration Packet, either the AES-CMAC digest or the RSA signature of the boot file is checked. As usual, if this final validation fails, the peripheral is reset and the ROM code jumps to the next NVM in the boot sequence.
If the boot file verification passes, the ROM code deciphers the boot file stored in the internal SRAM0.
Since the NVM interface is no longer needed, the ROM code restores the memory interface PIO and its settings to their reset values.
Finally, the ROM code locks access to the ROM area, enables JTAG and then branches to the beginning of the internal SRAM0 to execute the deciphered bootstrap.