47.3 External Analog Reference Connections
The following schematic checklist is only necessary if the application is using one or more of the external analog references. If the internal references are used instead, the following two circuits are not necessary.
| Signal Name | Recommended Pin Connection | Description |
|---|---|---|
| VREFA/VREFB | 1.0V to (VDDANA - 0.6V) for ADC
Decoupling capacitors 100nF(1)(2) and 4.7µF(1) | External reference VREFA/VREFBfor the analog port |
| GND | Ground |
1. These values are only given as a typical example.
2. Decoupling capacitor should be placed close to the device for each supply pin pair in the signal group.