3.6 LEDs
The on-board LEDs are categorized into two types:The following table provides details about the list of LEDs that the user can turn
ON or OFF while using the connected GPIO pins:
| Function | Description | Pin on the ATA8510 RF Board |
|---|---|---|
| Red LED (D102) | Remappable peripheral/PORTB digital I/O | PB7 |
| Green LED (D103) | Remappable peripheral/PORTC digital I/O | PC5 |