5.1 Setting Up the Hardware
(Ask a Question)Setting up the hardware involves interfacing the camera sensor module and the HDMI monitor with the PolarFire SoC video kit.
To set up the hardware, perform the following steps:
- Connect the camera sensor module at J10 on the video kit.
- Connect the HDMI monitor at J14 on the video kit using the HDMI cable.
- Ensure that the jumpers are set correctly on the video kit, as listed in the following table. For more information about the default jumper settings, see the "Jumper Settings" section in PolarFire SoC FPGA Video Kit User Guide.
| Jumper | Default Position | Functionality |
|---|---|---|
| J46 | 9 and 10 | Bank 1 voltage for UART communication |
| J40 | 9 and 10 | Bank 9 voltage |
| J2 and J3 | Open | DDR4 ref voltage |
| J20 | 1 and 2 | VBUS for FlashPro 6 |
| J23 | 1 and 2 | Backlight LED driver VANODE |
| J29 | Open | External on-board SPI Flash |
| J27 | Open | JTAG TRSTB |
| J39 | 12V Input | 12V input to Board |
| J28 | 1 and 2 | embedded Flash Programmer 6 (eFP6) |
| J41 | 1 and 2 | MSS reference 125 MHz clock |
| J9 | Open | MSS DDR Vref |
| J33 | 1 and 2 | VDDAUX9 3.3V |
| J30 | 1 and 2 | VDDAUX1 3.3V |
| J18 | Open | USB ID |
| J57 | Open | USB VBUS |
| J44 | 1 and 2 | Core voltage 1.05V |
The following figure shows the jumpers on the PolarFire SoC video kit.