5.3 Programming the Device
(Ask a Question)This section describes how to program the PolarFire SoC device, with the .job file, using FlashPro Express.
To program the device, perform the following steps:
- Connect a micro USB to J5 from the host PC and launch the FlashPro Express software from its installation directory.
- To create a new job project on the Project menu, click New or New Job Project from FlashPro Express Job.
- In the New Job Project dialog box, perform the following steps:
- Programming job file: Click Browse, navigate to the location where the
.jobfile is located, and select the file. The default location is: <download_folder\mpfs_an4723_v20xxpx_jb\mpfs_an4723_v20xxpx_df. - FlashPro Express job project location: Click Browse and navigate to the location where you want to save the project.
- Programming job file: Click Browse, navigate to the location where the
- Click OK. The required programming file is selected and ready to be programmed in the device. The FlashPro Express window appears. Verify that a programmer number (for example, 79DE6C53) appears in the Programmer field. If it does not, confirm the board connections and click Refresh/Rescan Programmers.
- To program the device, click RUN. When the device is programmed successfully, a RUN PASSED status is displayed.
- To close FlashPro Express, click .
- Power cycle the board using the SW5 switch.