46.7.3.11 Receiver Timeout

The Receiver Timeout provides support in handling variable-length frames. This feature detects an idle condition on the RXD line. When a timeout is detected, the FLEX_US_CSR.TIMEOUT bit rises and can generate an interrupt, thus indicating to the driver an end of frame.

The timeout delay period (during which the receiver waits for a new character) is programmed in the TO field of the Receiver Timeout register (FLEX_US_RTOR). If the TO field is written to 0, the Receiver Timeout is disabled and no timeout is detected. The FLEX_US_CSR.TIMEOUT bit remains at 0. Otherwise, the receiver loads a 16-bit counter with the value programmed in TO. This counter is decremented at each bit period and reloaded each time a new character is received. If the counter reaches 0, the FLEX_US_CSR.TIMEOUT bit rises. Then, the user can either:

  • Stop the counter clock until a new character is received. This is performed by writing a ‘1’ to FLEX_US_CR.STTTO. In this case, the idle state on RXD before a new character is received does not provide a timeout. This prevents having to handle an interrupt before a character is received and enables waiting for the next idle state on RXD after a frame is received.
  • Obtain an interrupt while no character is received. This is performed by writing a ‘1’ to FLEX_US_CR.RETTO. In this case, the counter starts counting down immediately from the value TO. This generates a periodic interrupt so that a user timeout can be handled, for example when no key is pressed on a keyboard.

The following figure shows the block diagram of the Receiver Timeout feature.

Figure 46-23. Receiver Timeout Block Diagram

The following table gives the maximum timeout period for some standard baud rates.

Table 46-9. Maximum Timeout Period
Baud Rate (bit/s) Bit Time (μs) Timeout (ms)
600 1,667 109,225
1,200 833 54,613
2,400 417 27,306
4,800 208 13,653
9,600 104 6,827
14,400 69 4,551
19,200 52 3,413
28,800 35 2,276
38,400 26 1,704
56,000 18 1,170
57,600 17 1,138
200,000 5 328