50.21 SDMMC Normal Interrupt Status Register (e.MMC)
| Name: | SDMMC_NISTR (EMMC) |
| Offset: | 0x30 |
| Reset: | 0x0000 |
| Property: | Read/Write |
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | |
| ERRINT | BOOTAR | ||||||||
| Access | R | R/W | |||||||
| Reset | 0 | 0 |
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
| BRDRDY | BWRRDY | DMAINT | BLKGE | TRFC | CMDC | ||||
| Access | R/W | R/W | R/W | R/W | R/W | R/W | |||
| Reset | 0 | 0 | 0 | 0 | 0 | 0 |
Bit 15 – ERRINT Error Interrupt
If any of the bits in SDMMC_EISTR are set, then this bit is set. Therefore, the user can efficiently test for an error by checking this bit first. This bit is read-only.
| Value | Description |
|---|---|
| 0 | No error. |
| 1 | Error. |
Bit 14 – BOOTAR Boot Acknowledge Received
This bit is set to '1' when the SDMMC received a Boot Acknowledge pattern from the e.MMC.
This bit can only be set to '1' if SDMMC_NISTER.BOOTAR is set to '1'. An interrupt can only be generated if SDMMC_NISIER.BOOTAR is set to '1'.
Writing this bit to '1' clears the bit.
| Value | Description |
|---|---|
| 0 |
Boot Acknowledge pattern not received. |
| 1 |
Boot Acknowledge pattern received. |
Bit 5 – BRDRDY Buffer Read Ready
This status is set to '1' if Buffer Read Enable (BUFRDEN) changes from '0' to '1'. See Buffer Read Enable (BUFRDEN) in SDMMC_PSR. While processing the tuning procedure (Execute Tuning (EXTUN) in SDMMC_HC2R is set to '1'), BRDRDY is set to '1' for every CMD19 execution.
This bit can only be set to '1' if SDMMC_NISTER.BRDRDY is set to '1'. An interrupt can only be generated if SDMMC_NISIER.BRDRDY is set to '1'.
Writing this bit to '1' clears the bit.
| Value | Description |
|---|---|
| 0 | Not ready to read buffer. |
| 1 | Ready to read buffer. |
Bit 4 – BWRRDY Buffer Write Ready
This status is set to 1 if Buffer Write Enable (BUFWREN) changes from '0' to '1'. See Buffer Write Enable (BUFWREN) in SDMMC_PSR.
This bit can only be set to '1' if SDMMC_NISTER.BWRRDY is set to '1'. An interrupt can only be generated if SDMMC_NISIER.BWRRDY is set to '1'.
Writing this bit to '1' clears the bit.
| Value | Description |
|---|---|
| 0 | Not ready to write buffer. |
| 1 | Ready to write buffer. |
Bit 3 – DMAINT DMA Interrupt
This status is set if the SDMMC detects the Host SDMA Buffer boundary during transfer. See SDMA Buffer Boundary (BOUNDARY) in SDMMC_BSR.
In case of ADMA, by setting “int” field in the descriptor table, the SDMMC raises this status flag when the descriptor line is completed. This status flag does not rise after the Transfer Complete (TRFC).
This bit can only be set to '1' if SDMMC_NISTER.DMAINT is set to '1'. An interrupt can only be generated if SDMMC_NISIER.DMAINT is set to '1'.
Writing this bit to '1' clears the bit.
| Value | Description |
|---|---|
| 0 | No DMA interrupt. |
| 1 | DMA interrupt. |
Bit 2 – BLKGE Block Gap Event
If the Stop At Block Gap Request (STPBGR) in SDMMC_BGCR is set to '1', this bit is set when either a read or a write transaction is stopped at a block gap. If STPBGR is not set to '1', this bit is not set to '1'.
In the case of a Read transaction:
This bit is set at the falling edge of the DAT Line Active (DLACT) status (when the transaction is stopped at SD bus timing). The Read Wait must be supported in order to use this function. See section “Read Transaction Wait / Continue Timing” in the “SD Host Controller Simplified Specification V3.00” about the detailed timing.
In the case of a Write transaction:
This bit is set at the falling edge of the Write Transfer Active (WTACT) status (after getting the CRC status at SD bus timing). See section “Write Transaction Wait / Continue Timing” in the “SD Host Controller Simplified Specification V3.00” for more details on the sequence of events.
This bit can only be set to '1' if SDMMC_NISTER.BLKGE is set to '1'. An interrupt can only be generated if SDMMC_NISIER.BLKGE is set to '1'.
Writing this bit to '1' clears the bit.
| Value | Description |
|---|---|
| 0 | No block gap event. |
| 1 | Transaction stopped at block gap. |
Bit 1 – TRFC Transfer Complete
This bit is set when a read/write transfer and a command with Busy is completed.
In the case of a Read Transaction:
This bit is set at the falling edge of the Read Transfer Active Status. The interrupt is generated in two cases. The first is when a data transfer is completed as specified by the data length (after the last data was read to the system). The second is when data has stopped at the block gap and completed the data transfer by setting the Stop At Block Gap Request (STPBGR) in SDMMC_BGCR (after valid data was read to the system). See section “Read Transaction Wait / Continue Timing” in the “SD Host Controller Simplified Specification V3.00” for more details on the sequence of events.
In the case of a Write Transaction:
This bit is set at the falling edge of the DAT Line Active (DLACT) status. This interrupt is generated in two cases. The first is when the last data is written to the card as specified by the data length and the Busy signal is released. The second is when data transfers are stopped at the block gap by setting Stop At Block Gap Request (STPBGR) in SDMMC_BGCR and data transfers are completed. (After valid data is written to the card and the Busy signal is released). See section “Write Transaction Wait / Continue Timing” in the “SD Host Controller Simplified Specification V3.00” for more details on the sequence of events.
In the case of command with Busy:
This bit is set when Busy is deasserted. See DAT Line Active (DLACT) and Command Inhibit (DAT) (CMDINHD) in SDMMC_PSR.
This bit can only be set to '1' if SDMMC_NISTER.TRFC is set to '1'. An interrupt can only be generated if SDMMC_NISIER.TRFC is set to '1'.
Writing this bit to '1' clears the bit.
The table below shows that Transfer Complete (TRFC) has a higher priority than Data Timeout Error (DATTEO). If both bits are set to '1', execution of a command can be considered to be completed.
| TRFC | DATTEO | Status Meaning |
|---|---|---|
| 0 | 0 | Interrupted by another factor |
| 0 | 1 | Timeout occurred during transfer |
| 1 | Don’t Care | Command execution complete |
| Value | Description |
|---|---|
| 0 | Command execution is not complete. |
| 1 | Command execution is complete. |
Bit 0 – CMDC Command Complete
This bit is set when getting the end bit of the command response. Auto CMD12 and Auto CMD23 consist of two responses. Command Complete is not generated by the response of CMD12 or CMD23, but it is generated by the response of a read/write command. See CMRINHC in SDMMC_PSR for details on how to control this bit.
This bit can only be set to '1' if SDMMC_NISTER.CMDC is set to '1'. An interrupt can only be generated if SDMMC_NISIER.CMDC is set to '1'.
Writing this bit to '1' clears the bit.
The table below shows that Command Timeout Error (CMDTEO) has a higher priority than Command Complete (CMDC). If both bits are set to '1', it can be considered that the response was not received correctly.
| CMDC | CMDTEO | Status Meaning |
|---|---|---|
| 0 | 0 | Interrupted by another factor |
| Don’t care | 1 | Response not received within 64 SDCLK cycles |
| 1 | 0 | Response received |
| Value | Description |
|---|---|
| 0 | No command complete. |
| 1 | Command complete. |