5.5.9 Read ADC Input Voltage (@,4)
Format:
@,4
Read the current voltage level. The unit of response is 0.001V. An analog signal can be
provided as an input to the RNBD350 module at
the ADC pin (PB1). The RNBD350 module does the
ADC conversion using a fixed reference and provides the digital value. Prior to
initiating the Read ADC Input Voltage command, the user has to
configure the factors of voltage detection using the Set ADC reference Factors
command (S@,<hex16>,<hex8>) command. Use the factors to get the
actual ADC voltage. This command expects the reference voltage and bias voltage
percentage as input parameters. For more details, refer to Set ADC Reference Factors (S@,<hex16>,<hex8>).
| Example: | @,4
| // Read battery voltage |
| Response: | 0A28 | // The analog value of 0A28 corresponds to the analog voltage of 2.6V |