5.5.1 Set UART Baud Rate (SB,<H8>,<H8>,<H8>, <H8>)
Format:
SB,<hex8>[,<00-01>,<00-03>,<00,01>]
This command sets the baud rate of the UART communication. The user can query the existing
configuration values using the
GB command. The input parameter is an
8-bit hex value in the range of 00-0B, representing baud rate from
2400-921600 (see the following table). The SB command also supports
three optional parameters to configure the UART parity and stop bits. - The first parameter sets the desired baud rate.
- The second parameter decides to Enable/Disable parity.
- Use the third parameter to set the Parity mode (see Table 5-29).
- The fourth parameter sets the desired stop bits.
|
Setting |
Baud Rate |
|---|---|
00 | 921600 |
01 | 460800 |
02 | 230400 |
03 | 115200 |
04 | 57600 |
05 | 38400 |
06 | 28800 |
07 | 19200 |
08 | 14400 |
09 | 9600 |
0A | 4800 |
0B | 2400 |
The second parameter is used to enable or disable the parity check (see the following table).
| Setting | Parity Check |
|---|---|
| 00 | Disable |
| 01 | Enable |
The third parameter is used to select the Parity mode (see the following table), which works only after enabling the parity check.
| Setting | Mode |
|---|---|
| 00 | Odd |
| 02 | Even |
| Setting | Stop Bits |
|---|---|
| 00 | 1 |
| 01 | 2 |
| Default: | 03 | |
| Example: | SB,07
| // Set the UART baud rate to 19200 |
SB,04,01,02,00
| // Set the UART baud rate to 57600 | |
| // Enable the parity check as Even mode | ||
| // Set the stop bits to 1 bit | ||
| Response: | AOK
| // Success |
Err | // Syntax error or invalid parameter | |
|
Note: The PDS stores
these parameters. The parameters are effective after reboot.
| ||