The following are the steps to launch the Microchip RNBD Utility tool:
To launch the tool, double click RNBD_DFU_OTAPC_Vx.x.x.exe.
The tool has two separate tabs for each feature. By default, the DFU tab is selected.
From the “Serial Ports” drop-down list, select the respective COM Port.
From the “Baud Rate” drop down list, select the baud rate. For example, select 115200.
Click Connect to continue.Figure 8-5. Microchip RNBD Utility Tool Serial DFU Tab View
After clicking the Connect button, the following buttons become active:
Browse
Disconnect
The OTAPC tab is grayed out.
If the connection is successful, the console text log displays the COM port and baud rate.
Figure 8-6. Microchip RNBD Utility Tool Serial DFU Tab Connection Established
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.