8.4.5.1 Launch the Tool
The following are the steps to launch the Microchip RNBD Utility tool:
- To launch the tool, double click
RNBD_DFU_OTAPC_Vx.x.x.exe. - The tool has three separate tabs for each feature. By default, the DFU tab is selected and need to select OTA DFU tab for the Firmware upgrade using mobile app.
- From the “Serial Ports” drop-down list, select the respective COM Port.
- From the “Baud Rate” drop down list, select the baud rate. For example, select 115200.
- Click Connect to continue.
Figure 8-22. Microchip RNBD Utility Tool OTA DFU Tab View
- After clicking the Connect button,
the following buttons become active:
- Update
- Disconnect
The Serial DFU and OTAPC tab is grayed out.
- If the connection is successful, the
console text log displays the COM port and baud rate.
Figure 8-23. Microchip RNBD Utility Tool OTA DFU Tab Connection Established
- Click the Update button. Upon clicking the update button the tool will be ready for OTA DFU procedure.
Figure 8-24. RNBD350 Device Connection Request Message