5.8 data_alignment Pragma
It gives immediately following variable a stricter alignment of the start address.
On XC32, the closest representation to is ___attribute__((aligned))
which has a similar granularity.
Pack instead applies the specified alignment to all structs after its definition and not only the one immediately after it.
Suggested Replacement
___attribute__((aligned(n)))
Caveats
None.
Examples
Consider migrating IAR code such
as:
#pragma data_alignment=2to MPLAB XC codes similar
to:__attribute__((aligned (2))) Further Information
None.