5.25 Inline Pragma
Use #pragma inline to advise the compiler that the function defined immediately after the directive should be inlined according to C++ inline semantics.
XC32 only has an equivalence for inline with no parameters. But other keywords cover the same functionality.
Note: The inline keyword will only be recognized with
-finline or optimizations enabled. To replicate the functionality of forcing inlining then use "always_inline". To replicate the "never" parameter then use "never_inline".Suggested Replacement
inline
always_inline
never_inline
Caveats
None.
Examples
Consider migrating IAR code such as:
#pragma inline[=forced|=never]to MPLAB XC codes similar to:inline void foo();Further Information
None.