5.27 Location Pragma
Use this pragma directive to specify:
- The location—the absolute address—of the global or static variable whose
declaration follows the pragma directive. The variables must be declared
__no_init. - An identifier specifying a register. The variable defined after the pragma
directive is placed in the register. The variable must be declared as
__no_initand have file scope.
Note: There is no support in XC32 to set value to specific register.
Suggested Replacement
__attribute__((section, address))
Caveats
None.
Examples
Consider migrating IAR code such
as:
#pragma location=0xFFFF0400 __no_init volatile char PORT1; to
MPLAB XC codes similar
to:int foo __attrribute__((section("mysection"), address(0xA0001000)))Further Information
None.