5.50 Weak Pragma
The weak attribute causes the declaration to be emitted as a weak symbol. A weak symbol indicates that if a global version of the same symbol is available, that version should be used instead.
Suggested Replacement
__attribute__((weak))
Caveats
None.
Examples
Consider migrating IAR code such as:
#pragma weak footo MPLAB
XC codes similar to:extern int __attribute__((weak)) s;Further Information
None.