5.3.2 SAM E70 Xplained Ultra Evaluation Kit
In this section, only fractional baud rate part will be explained whereas the remaining
are the same as the Basic configuration section. Fractional baud rate of 11000 bps is used in
the application. The macro FRAC_BAUD_RATE contains the fractional baud
value. Adhere to the steps outlined for the basic configuration of the SAM E70 Xplained
Ultra Evaluation Kit. The following figure illustrates the block diagram.
Note: Click here to access the source code for this
application configuration. Alternatively, it is also available in the GitHub reference_apps repository.