4.2.1 Programming the Device Using FlashPro Express
(Ask a Question)This section describes how to program the PolarFire device with the .job file using FlashPro Express. The .job file is downloaded using the following link:
www.microchip.com/en-us/application-notes/AN5488
To program the PolarFire device with the .job file, follow these steps:
- On the host PC, start the FlashPro Express software from its installation directory.
- To create a new job project, select New or New Job Project from FlashPro Express Job from Project menu.
- Enter the following details in the New Job Project from FlashPro Express Job dialog box:
- Programming the job file: Click
Browse and navigate to the location where the
.jobfile is located and select the file. The default location is: <$Download_Directory>\mpf_an5488_v2024p1_df\Programming_job - FlashPro Express job project location: Select Browse and navigate to the location where you want to save the project.
- Programming the job file: Click
Browse and navigate to the location where the
- Click OK. The required programming
.jobfile is selected and ready to be programmed in the device. - Confirm that a programmer number appears in the Programmer field. If it does not, confirm the board connections and click Refresh/Rescan Programmers.
- Click RUN to program the device. When the device is programmed successfully, a RUN PASSED status is displayed. See Running the Demo.