36.4.1.3.1 Client Transmission (7-bit Addressing Mode)
The following section describes the sequence of events that occur when the module is transmitting data in 7-bit Addressing mode:
- The host device issues a Start condition. Once the Start condition has been detected, client hardware sets the Start Condition Interrupt Flag (SCIF) bit. If the Start Condition Interrupt Enable (SCIE) bit is also set, the generic I2CxIF is also set.
- Host hardware transmits the 7-bit client address with the R/W bit set, indicating that it intends to read data from the client.
- The received address is compared to
the values in the I2CxADR registers. If the client is configured in 7-bit Addressing
mode (no masking), the received address is independently compared to each of the
I2CxADR0/1/2/3 registers. In 7-bit Addressing with Masking mode, the received
address is compared to the masked value of I2CxADR0
and I2CxADR2.
If an address match occurs:
- The Client mode Active (SMA) bit is set by module hardware.
- The R/W bit value is copied to the Read Information (R) bit by module hardware.
- The Data (D) bit is cleared by hardware, indicating the last received byte was an address.
- The Address Interrupt Flag (ADRIF) bit is set. If the Address Interrupt and Hold Enable (ADRIE) bit is set and the Clock Stretching Disable (CSD) bit is clear, hardware sets the Client Clock Stretching (CSTR) bit and the generic I2CxIF bit. This allows time for the client to read either I2CxADB0 or I2CxRXB and selectively ACK/NACK based on the received address. When the client has finished processing the address, software must clear CSTR to resume operation.
- The matching received address
is loaded into either the I2CxADB0 register or into the I2CxRXB register as
determined by the Address Buffer Disable (ABD) bit. When ABD is clear (ABD =
0), the matching address is copied to I2CxADB0. When ABD is set (ABD =1), the matching address is copied to I2CxRXB, which also sets the Receive Buffer Full Status (RXBF) bit and the I2C Receive Interrupt Flag (I2CxRXIF) bit. I2CxRXIF is a read-only bit and must be cleared by either reading I2CxRXB or by setting the Clear Buffer (CLRBF) bit (CLRBF =1).
If no address match occurs, the module remains idle.
- If the Transmit Buffer Empty Status
(TXBE) bit is set (TXBE =
1), I2CxCNT has a non-zero value (I2CxCNT !=0), and the I2C Transmit Interrupt Flag (I2CxTXIF) is set (I2CxTXIF =1), client hardware sets CSTR, stretches the clock (when CSD =0), and waits for software to load I2CxTXB with data. I2CxTXB must be loaded to clear I2CxTXIF. Once data are loaded into I2CxTXB, hardware automatically clears CSTR to resume communication. - The host device transmits the 9th
clock pulse, and client hardware transfers the value of the ACKDT bit onto the SDA line. If there are pending errors,
such as a receive overflow (RXO =
1), client hardware automatically generates a NACK condition. NACKIF is set, and the module goes idle. - Upon the 9th falling SCL edge, the
data byte in I2CxTXB is transferred to the transmit shift register, and I2CxCNT is
decremented by one. Additionally, the Acknowledge Status Time Interrupt Flag (ACKTIF) bit is set. If the Acknowledge Status Time
Interrupt and Hold Enable (ACKTIE) bit is also set, the generic I2CxIF is set, and if
client hardware generated an ACK, the CSTR bit is also set and the clock is stretched (when CSD =
0). If a NACK was generated, the CSTR bit remains unchanged. Once complete, software must clear CSTR and ACKTIF to release the clock and continue operation. - If the client generated an ACK and I2CxCNT is non-zero, host hardware transmits eight clock pulses, and client hardware begins to shift the data byte out of the shift register starting with the Most Significant bit (MSb).
- After the 8th falling edge of SCL,
client hardware checks the status of TXBE and I2CxRXB. If TXBE is set and I2CxCNT has a non-zero
count value, hardware sets CSTR and the clock is stretched (when CSD =
0) until software loads I2CxTXB with new data. Once I2CxTXB has been loaded, hardware clears TXBE, I2CxTXIF, and CSTR to resume communication. - Once the host hardware clocks in all
eight data bits, it transmits the 9th clock pulse along with the
ACK/NACK response back to the client. Client hardware
copies the ACK/NACK value to the Acknowledge Status (ACKSTAT) bit and sets ACKTIF. If ACKTIE is also set, client hardware sets the generic I2CxIF bit and
CSTR and stretches the clock (when CSD
=
0). Software must clear CSTR to resume operation. - After the 9th falling edge of SCL,
data currently loaded in I2CxTXB is transferred to the transmit shift
register, setting both TXBE and I2CxTXIF. I2CxCNT is decremented by
one. If I2CxCNT is zero (I2CxCNT =
0), CNTIF is set. - If I2CxCNT is non-zero and the host
issued an ACK on the last byte (ACKSTAT =
0), the host transmits eight clock pulses, and client hardware begins to shift data out of the shift register. - Repeat steps 8 – 11 until the host
has received all the requested data (I2CxCNT =
0). Once all data have been received, the host issues a NACK, followed by either a Stop or Restart condition. Once the NACK has been received by the client, hardware sets NACKIF and clears SMA. If the NACK Detect Interrupt Enable (NACKIE) bit is also set, the generic I2C Error Interrupt Flag (I2CxEIF) is set. If the host issued a Stop condition, client hardware sets the Stop Condition Interrupt Flag (PCIF). If the host issued a Restart condition, client hardware sets the Restart Condition Interrupt Flag (RSCIF). If the associated interrupt enable bits are also set, the generic I2CxIF is also set.Important: I2CxEIF is read-only and is cleared by hardware when all enable interrupt flag bits in I2CxERR are cleared.
1)1)