Running an AI Digit Recognition Application
To run an AI digit recognition application, after programming with the
Demo3_
HF10_DIGIT_CNN_FF_Vxx.dat file, perform the following steps:- Click the FPGA
Demo tab. The FPGA captures the video from camera and runs
Convolution Neural Network (CNN) to recognize the digit in the video stream.
Figure . Digit Recognition
- Point the camera to align green box around a digit with the green box on the LCD. The recognized digit is displayed on the LCD, and on the left side of the GUI window.
- Use Digit Set 1, Digit Set 2, or Digit Set 3 to test with different fonts.