31.2.1 Starting a Conversion
To enable the ADC module, the ADON must be set to a ‘1’. A conversion may be started by any of the following:
- Software setting the ADGO bit to '1'
- An external trigger (source selected by ADACT)
- A continuous-mode retrigger (see section Continuous Sampling Mode)
.
Important: The ADGO bit should not be set in the same instruction that turns on the ADC. Refer to ADC Conversion Procedure (Basic Mode).