11.1.2 Return Address Stack
The return address stack allows any combination of up to 31 program
         calls and interrupts to occur. The PC is pushed onto the stack when a CALL
         or RCALL instruction is executed or an interrupt is Acknowledged. The PC
         value is pulled off the stack on a RETURN, RETLW or a
            RETFIE instruction. PCLATU and PCLATH are not affected by any of the
            RETURN or CALL instructions.
The stack operates as a 31-word by 21-bit RAM and a 5-bit Stack Pointer, or as a 35-word by 21-bit RAM with a 6-bit Stack Pointer in ICD mode. The stack space is not part of either program or data space. The Stack Pointer is readable and writable and the address on the top of the stack is readable and writable through the Top-of-Stack (TOS) Special File registers. Data can also be pushed to, or popped from the stack, using these registers.
A CALL type instruction causes a push onto the
         stack; the Stack Pointer is first incremented and the location pointed to by the Stack
         Pointer is written with the contents of the PC (already pointing to the instruction
         following the CALL). A RETURN type
         instruction causes a pop from the stack; the contents of the location pointed to by the
         STKPTR are transferred to the PC and then the Stack Pointer is decremented.
The Stack Pointer is initialized to ‘0b00000’ after all Resets. There is no RAM associated with the location corresponding to a Stack Pointer value of ‘0b00000’; this is only a Reset value. Status bits in the PCON0 register indicate if the stack is full or has overflowed or has under-flowed.