4.4 Creating a New MCC Harmony Project

  1. To create a new project, open MPLAB X IDE and click on File>New Project.
    Figure 4-4. New Project
  2. In the “New Project” pop-up, click on Microchip Embedded>Application Project(s)>Next.
    Figure 4-5. Choose Project
  3. In Select Device window, select the device from drop down and click Next.
    Figure 4-6. Select Device
  4. In Select Compiler window, Select the latest compiler and click Next.
    Figure 4-7. Select Compiler
  5. In Select Project Name and Folder window, enter the project name and select the project location, and click Finish.
    Figure 4-8. Select Project Name and Folder
  6. Now MPLAB X Code Configurator Content Manager will be launched automatically. It will setup the configuration and initiate the project.
    Figure 4-9. MCC Required Content
    1. After a while, MCC will display the project graph containing the default component: CMSIS Pack, System, Device Family Pack and EVSYS.
      Figure 4-10. Project Graph
    2. Project and Device resources.
      Figure 4-11. Project and Device resources