5.6 Customer Tab
The following figure illustrates the Customer Settings within the Customer tab for
setting up the customer-defined parameters within the EEPROM. The check box for the
Export Customer Settings allows the storage of these settings in the
*.hex programmer file.
Note: There are no default settings;
therefore, all values are unassigned with 0xFF.