4 EEPROM Configuration Tool Setup
The following are the sequence of steps for setting up an EEPROM
configuration:
- Load the default configuration. For more details, refer to EEPROM Configuration Tool Installation.
- Modify the EEPROM configuration according to the application requirements, such as RF, Data Rate (DR), coding, pattern and more.
- Store the new configuration in a
.xmlfile format for later reload into the EEPROM configuration tool. For programming purposes, store the configuration in a.hexfile format or any of the other available formats.