1.22 RTC tamper detect
This example application shows how to configure and use tamper detect feature of RTC.
Description
This example application shows how to setup system time and configure tamper detection using the RTC Peripheral Library. The application sets up system time and then waits for tamper detection to happen. On Tamper detection, application displays the tamper detected information and timestamp at which tamper is detected.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/rtc/rtc_tamper_detect/.
To build the application, refer to the following table and open the project using its IDE.
Project Name | Description |
---|---|
pic32cm_gc_curiosity_pro.X | MPLABX project for PIC32CM GC00 Curiosity Pro Board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
Project Name | Description |
---|---|
pic32cm_gc_curiosity_pro.X | PIC32CM GC00 Curiosity Pro Board |
Setting Up PIC32CM GC00 Curiosity PRO Board
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Open the Terminal application (Ex.:Tera term) on the computer.
- Connect to the PKOB4 Virtual COM port and configure the serial settings as
follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
- Build and Program the application project using its IDE.
- System time is displayed in
terminal session as RTC is configured in calendar mode.
- To generate a tamper event, press switch.
- Upon detection of the tamper
event, LED will be toggled and the console output will be updated as
follows:
Board | Switch Name | LED Name |
---|---|---|
PIC32CM GC00 Curiosity Pro Board | SW0 | LED0 |