1 MPLAB® Harmony 3 Peripheral Library Application Examples for PIC32CM-GC/SG Family
The following applications are provided to demonstrate the typical or interesting usage models of one or more peripheral libraries.
| Name | Description |
|---|---|
| AC Sleepwalking | This example application shows how to use the AC Peripheral library to perform a single shot comparison in standby sleep mode periodically and wake up the device when the comparator output toggles. |
| ADC Blocking | This example application shows how to use the ADC Peripheral library in blocking mode to convert analog input on a ADC channel. |
| ADC DMA Scan | This example application shows how to use the ADC Peripheral library in scan mode to convert multiple analog input on a ADC channels and transfer the ADC result using DMA. |
| ADC Interrupt | This example application shows how to use the ADC Peripheral library in interrupt mode to convert multiple analog inputs. |
| CAN FD Blocking | This example application shows how to use the CAN module to transmit and receive CAN FD messages in polling mode. |
| CAN FD Interrupt | This example application shows how to use the CAN module to transmit and receive CAN FD messages in interrupt mode |
| Clock Configuration | This example application shows how to configure the clock system to run the device at maximum frequency. It also outputs a prescaled clock signal on a GPIO pin for measurement and verification. |
| DMAC CRC-32 Generation | This example application demonstrates how to use the DMAC peripheral to compute 32-bit Cyclic Redundancy Checksum (CRC). |
| DMAC Memory Transfer | This example application demonstrates how to use the DMAC peripheral to do a memory to memory transfer. |
| DMAC USART Echo | This example application demonstrates USART transfer with DMA to receive 10 bytes and echo back the received bytes. |
| EIC Interrupt | This example application demonstrates how to generate interrupt using the EIC on switch press and indicate it through an LED. |
| EVSYS Trigger | This example application demonstrates how to use the EVSYS Peripheral library to setup autonomous, low-latency and configurable communication between peripherals. |
| FCW Read Write | This example application demonstrates how to use the FCW to erase and program the internal Flash memory. |
| FREQM Measurement | This example application demonstrates how to use the FREQM peripheral to measure the frequency of the internal RC Oscillator. |
| MCRAMC ECC with Fault Injection Testing | This example application demonstrates how to test the SRAM using the MCRAMC ECC feature on internal SRAM memory. |
| PM Wakeup using EIC | This example demonstrates entering the low power modes and exiting it using the EIC. |
| PM Wakeup using RTC | This example demonstrates entering the low power modes and exiting it using the RTC. |
| PORT Polling | This example application demonstrate how to poll the switch input, and indicate the switch status using the LED. |
| RSTC Reset Cause | This example shows how to use the RSTC peripheral to indicate the cause of the device reset. |
| RTC Alarm Interrupt | This example shows how to use the RTC to configure the time and generate the alarm. |
| RTC Periodic Interrupt | This example application shows how to use the RTC to generate periodic interrupts. |
| RTC Tamper Detect | This example application shows how to configure and use tamper detect feature of RTC. |
| SERCOM I2C EEPROM Read Write | This example application demonstrates how to use the SERCOM peripheral to write and read from the I2C serial EEPROM memory. |
| SERCOM SPI EEPROM Read Write | This example application demonstrates how to use the SERCOM SPI peripheral to write and read from the SPI serial EEPROM memory. |
| SERCOM SPI Interrupt | This example application shows how to use SERCOM SPI PLIB with external loop back to write and then read back an array of data in interrupt mode. |
| SERCOM USART Blocking | This example application demonstrates how to use the SERCOM peripheral in USART mode to transfer block of data in a blocking manner. |
| SERCOM USART Interrupt | This example application demonstrates how to use the SERCOM peripheral in USART mode to transfer data in a non-blocking manner. |
| SERCOM USART Ring Buffer | This example application demonstrates how to use the SERCOM peripheral in USART ring buffer mode to transfer data in a non-blocking manner. |
| Systick Periodic Interrupt | This example shows how to use the SysTick to generate periodic interrupts. |
| TCC Capture Mode | This example shows how to use the TCC module in capture mode to measure duty cycle and frequency of an external input. |
| TCC Compare Mode | This example shows how to use the TCC module in compare mode to generate different waveforms. |
| TCC Timer Mode | This example shows how to use the TCC module in timer mode to generate periodic interrupt. |
| Trustzone EIC Pin Toggle | This example application demonstrates handling of external pin interrupt in secure and non-secure project. |
| TrustZone Secure TCC Demonstration | This example application performs a PWM signal applied on LED0 based on TCC0 peripheral. |
| TrustZone Systick periodic timeout | This example application shows how to use the SysTick to generate periodic interrupts on both Secure and Non-secure modes. |
| WDT Timeout | This example shows how to generate a Watchdog timer reset by emulating a deadlock. |