1.20 RTC Alarm Interrupt
This example shows how to use the RTC to configure the time and generate the alarm.
Description
This example application shows how to setup system time and configure alarm using the RTC Peripheral Library. The application sets up an alarm to be generated after 20 seconds of the configured system time. The application displays a message on the alarm trigger.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/rtc/rtc_alarm/firmware/.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| pic32cm_gc_curiosity_pro.X | MPLABX project for PIC32CM GC00 Curiosity Pro Board | 
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description | 
|---|---|
| pic32cm_gc_curiosity_pro.X | PIC32CM GC00 Curiosity Pro Board | 
Setting Up PIC32CM GC00 Curiosity PRO Board
- Connect the Debug USB port on the board to the computer using a micro USB cable
 
Running the Application
- Open the Terminal application (Ex.:Tera term) on the computer.
 - Connect to the PKOB4 Virtual COM port and configure the serial settings as
                        follows:
- Baud : 115200
 - Data : 8 Bits
 - Parity : None
 - Stop : 1 Bit
 - Flow Control : None
 
 - Build and Program the application project using its IDE.
 - The console displays the current time and the alarm time (System time starts at
                    12:00:00 and gets updated every second).

 - Once the alarm time is reached, it print the alarm message and turns on the LED
                    (System time keeps updating).

 
| Board | LED Name | 
|---|---|
| PIC32CM GC00 Curiosity Pro Board | LED0 |