1.15 MCRAMC ECC with Fault Injection Testing
This example application demonstrates how to test the SRAM using the MCRAMC ECC feature on internal SRAM memory.
Description
This example uses the MCRAMC to test its ECC with Fault Injection feature. This application writes a 32-bit data in SRAM for single and double error injection to highlight SEC and DED process.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/mcramc/mcramc_ecc_testing/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32cm_gc_curiosity_pro.X | MPLABX project for PIC32CM GC00 Curiosity Pro Board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| pic32cm_gc_curiosity_pro.X | PIC32CM GC00 Curiosity Pro Board |
Setting Up PIC32CM GC00 Curiosity PRO Board
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Build and Program the application using its IDE.
- Application Menu is displayed with following choices.
- 'a': Single Fault Injection is chosen and following message is displayed
on console:

- 'b': Double Fault Injection is chosen and following message is displayed
on console:

- 'a': Single Fault Injection is chosen and following message is displayed
on console:
- The on-board LED blinks each time a SERR interrupt occurs.