1.3 ADC DMA Scan
This example application shows how to use the ADC Peripheral library in scan mode to convert multiple analog input on a ADC channels and transfer the ADC result using DMA.
Description
The example configures ADC0 channel 0 and channel 1 in scan mode. The scan trigger source is configured as ADC trigger event. RTC is configured to generate a periodic RTC compare match event. ADC trigger is configured as the user of the RTC compare match event. ADC starts conversion of channel 0 and channel 1 on every scan trigger and stores the result in the ADC FIFO. DMA is triggered whenever the ADC FIFO has ADC result. DMA reads the result from ADC FIFO and copies it to the user buffer. DMA interrupt is generated when results for both the channels are copied to the user buffer. The application prints the ADC count and the corresponding analog voltage on the serial terminal.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/adc/adc_dma_scan/firmware .
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32cm_gc_curiosity_pro.X | MPLABX project for PIC32CM GC00 Curiosity Pro Board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| pic32cm_gc_curiosity_pro.X | PIC32CM GC00 Curiosity Pro Board |
Setting Up PIC32CM GC00 Curiosity PRO Board
- Connect the Debug USB port on the board to the computer using a micro USB cable
- ADC Core 0 Channel 0 input is available on PA04 (Pin 3 of EXT1). Connect PA04 to analog input voltage.
- ADC Core 0 Channel 1 input is available on PA05 (Pin 4 of EXT1). Connect PA05 to analog input voltage.
Running the Application
- Build and Program the application using its IDE
- Connect to the PKOB4 Virtual COM port and configure the serial settings as
follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
- The demo application will print the ADC count and the corresponding analog
voltage measured on pin PA04 (Pin 3 of EXT1) and pin PA04 (Pin 4 of EXT1):