1.11 FILEX File System Using SST26 Media
This application shows an example of using the FILEX File System to access SQI based SST26 Flash media.
Description
File System Operations on the On-Board SST26 Flash Memory
- Performs a SYS_FS_FormatDisk
- Opens a
newfile.txton the SST26 Flash - Write and reads back 4 KB of
data on
newfile.txt - Verifies the Data Read back
File System Layer Uses
- One instance of the Memory driver is used to communicate with the on-board SQI Flash memory
Downloading and Building the Application
To clone or download this application from GitHub, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/fs/sqi_flash_filex/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_e54_xpro.X | MPLAB X project for SAM E54 Xplained Pro Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_e54_xpro.X | SAM E54 Xplained Pro Evaluation Kit |
Setting Up SAM E54 Xplained Pro Evaluation Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Build and program the application using its IDE.
- The LED is turned ON if data has
successfully been written and read back from file
newfile.txt.
Refer to the following table for LED name:
| Board | LED Name |
|---|---|
| SAM E54 Xplained Pro Evaluation Kit | LED0 |