1.8 FAT File System Using SD Card Media
This application shows an example of using the MPLAB Harmony File System to access and modify the contents of an SD card using the SDSPI driver and the SPI PLIB.
Description
File System Operations on the SD Card
- The application opens a file
named
FILE_TOO_LONG_NAME_EXAMPLE_123.JPGon the SD card - Reads the content of the file
and creates a directory named
Dir1 - Inside the directory, writes
the copied content into another file
Dir1/FILE_TOO_LONG_NAME_EXAMPLE_123.JPG
The image file could be any arbitrary JPEG (image) file chosen by the user and
then renamed to FILE_TOO_LONG_NAME_EXAMPLE_123.JPG. The reason
for choosing a JPEG file for test purposes is that the duplicate file,
Dir1/FILE_TOO_LONG_NAME_EXAMPLE_123.JPG created by the
demonstration could be easily verified for correctness.
If the new file inside Dir1 opens for viewing on the computer
and matches to original image, the test is deemed to have passed. Otherwise, if
the file does not open (i.e., is corrupted), the test will be considered to have
failed.
Dir1, it is important that the a folder with the same name
does not exist on the SD card. If a directory named Dir1 is
already present on the SD card, the application will fail.File System Layer Uses
SDSPI Driver to communicate to SD card over SPI interface.
Downloading and Building the Application
To clone or download this application from GitHub, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/fs/sdspi_fat/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_e54_xpro_freertos.X | MPLAB X project for SAM E54 Xplained Pro Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_e54_xpro_freertos.X | SAM E54 Xplained Pro Evaluation Kit |
Setting Up SAM E54 Xplained Pro Evaluation Kit
- To run the demo, the following additional hardware are required:
- I/O1 Xplained Pro Extension Kit
- microSD card formatted to FAT File System
- Connect the I/O1 Xplained Pro Extension Kit to the EXT1 header
- Copy a JPEG file in the SD
card with name
FILE_TOO_LONG_NAME_EXAMPLE_123.JPG - Insert microSD card on the I/O1 Xplained Pro Extension Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Build and program the application using its IDE.
- Press the switch to start the application.
- The LED is turned ON if there was
no error during creating the directory and copying the file into it.Refer to the following table for Switch and LED names:
Board Switch Name LED Name SAM E54 Xplained Pro Evaluation Kit SW0 LED0 - If LED is ON, insert the SD card on to the host PC.
- SD card should have the file
Dir1/FILE_TOO_LONG_NAME_EXAMPLE_123.JPGand should match the original image.