1.23 MPFS File System Using NVM Media

This application shows an example of implementing the MPFS disk in device internal Flash memory.

Description

File System Operations on NVM

  • The application contains the MPFS disk image in the internal Flash memory. The disk image contains two files named:
    • FILE.txt, Size = 11 bytes. The content of the file is: Hello World
    • TEST.txt, Size = 10 bytes. The content of the file is: 1234567890
  • The application performs following file system related operations:
    • SYS_FS_FileRead
    • SYS_FS_FileStat
    • SYS_FS_FileSize
    • SYS_FS_FileSeek
    • SYS_FS_FileEOF
  • The contents of both the files are read and compared with the expected strings as mentioned above. If the string compare is successful, an LED indication is provided.

File System Layer Uses

  • Memory driver to communicate with underlying NVM media

Downloading and Building the Application

To clone or download this application from GitHub, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/fs/nvm_mpfs/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sam_e54_xpro.XMPLAB X project for SAM E54 Xplained Pro Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
sam_e54_xpro.XSAM E54 Xplained Pro Evaluation Kit

Setting Up SAM E54 Xplained Pro Evaluation Kit

  • Connect the Debug USB port on the board to the computer using a micro USB cable

Running the Application

  1. Build and program the application using its IDE.
  2. The LED is turned ON when the following criteria is satisfied.
    • File FILE.txt has the string Hello World in it
    • File TEST.txt has the string 1234567890 in it
Refer to the following table for LED name: