1.6 FAT File System Using AT24 EEPROM Media

This application shows an example of using the MPLAB Harmony File System to access I2C EEPROM based media.

Description

File System Operations on the AT24 EEPROM Memory

  • Performs a SYS-FS_FormatDisk
  • Opens a newfile.txt on the I2C EEPROM media (AT24 EEPROM)
  • Write and reads back 4 KB of data on newfile.txt
  • Verifies the Data Read back

File System Layer Uses

  • Memory driver to communicate with external AT24 EEPROM device using I2C

Downloading and Building the Application

To clone or download this application from GitHub, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/fs/i2c_eeprom_fat/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sam_e54_xpro.XMPLAB X project for SAM E54 Xplained Pro Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
sam_e54_xpro.XSAM E54 Xplained Pro Evaluation Kit

Running the Application

  1. Build and program the application using its IDE.
  2. Press switch to start the operation.
  3. The LED is turned ON if writing and reading is successful on EEPROM media.
Refer to the following table for Switch and LED names:
BoardSwitch NameLED Name
SAM E54 Xplained Pro Evaluation KitSW0LED0