1.6.2.1 Bootloader Trigger Methods
Bootloader can be invoked in number of ways:
- Bootloader will run automatically if there is no valid application firmware
- Firmware is considered valid if the first word at application start address is not
0xFFFFFFFF
- Normally this word contains initial stack pointer value for MCUs, so it will never be 0xFFFFFFFF unless device is erased
- Bootloader application can implement the bootloader_Trigger() function
which will be called during system initialization
-
A GPIO pin can be used as an external trigger to invoke bootloader at startup
-
Bootloader can run on application (internal) request if the configured number of bytes from start of SRAM are equal to some trigger pattern (For MCUs)
-
Example Implementation of bootloader_Trigger()
#define BTL_TRIGGER_PATTERN 0x5048434D static uint32_t *ramStart = (uint32_t *)BTL_TRIGGER_RAM_START; bool bootloader_Trigger(void) { /* Check for Bootloader Trigger Pattern in first 16 Bytes of RAM to enter * Bootloader. */ if (BTL_TRIGGER_PATTERN == ramStart[0] && BTL_TRIGGER_PATTERN == ramStart[1] && BTL_TRIGGER_PATTERN == ramStart[2] && BTL_TRIGGER_PATTERN == ramStart[3]) { ramStart[0] = 0; return true; } /* Check for Switch press to enter Bootloader */ if (SWITCH_Get() == 0) { return true; } return false; }
Application code to trigger bootloader (For OTA bootloader and bootloaders for MPU devices)
bool bootloader_Trigger(void) { /* Check for Switch press to enter Bootloader */ if (SWITCH_Get() == 0) { return true; } return false; }
Application code to trigger bootloader
void invoke_bootloader(void) { uint32_t *sram = (uint32_t *)BTL_TRIGGER_RAM_START; sram[0] = 0x5048434D; sram[1] = 0x5048434D; sram[2] = 0x5048434D; sram[3] = 0x5048434D; NVIC_SystemReset(); }