14.1 Interrupt Vectors in ATmega324PB
| Vector No | Program Address(2) | Source | Interrupts definition |
|---|---|---|---|
| 1 | 0x0000(1) | RESET | External Pin, Power-on Reset, Brown-out Reset and Watchdog System Reset |
| 2 | 0x0002 | INT0 | External Interrupt Request 0 |
| 3 | 0x0004 | INT1 | External Interrupt Request 1 |
| 4 | 0x0006 | INT2 | External Interrupt Request 2 |
| 5 | 0x0008 | PCINT0 | Pin Change Interrupt Request 0 |
| 6 | 0x000A | PCINT1 | Pin Change Interrupt Request 1 |
| 7 | 0x000C | PCINT2 | Pin Change Interrupt Request 2 |
| 8 | 0x000E | PCINT3 | Pin Change Interrupt Request 3 |
| 9 | 0x0010 | WDT | Watchdog Time-out Interrupt |
| 10 | 0x0012 | TIMER2_COMPA | Timer/Counter2 Compare Match A |
| 11 | 0x0014 | TIMER2_COMPB | Timer/Coutner2 Compare Match B |
| 12 | 0x0016 | TIMER2_OVF | Timer/Counter2 Overflow |
| 13 | 0x0018 | TIMER1_CAPT | Timer/Counter1 Capture Event |
| 14 | 0x001A | TIMER1_COMPA | Timer/Counter1 Compare Match A |
| 15 | 0x001C | TIMER1_COMPB | Timer/Coutner1 Compare Match B |
| 16 | 0x001E | TIMER1_OVF | Timer/Counter1 Overflow |
| 17 | 0x0020 | TIMER0_COMPA | Timer/Counter0 Compare Match A |
| 18 | 0x0022 | TIMER0_COMPB | Timer/Coutner0 Compare Match B |
| 19 | 0x0024 | TIMER0_OVF | Timer/Counter0 Overflow |
| 20 | 0x0026 | SPI0_STC | SPI0 Serial Transfer Complete |
| 21 | 0x0028 | USART0_RX | USART0 Rx Complete |
| 22 | 0x002A | USART0_UDRE | USART0, Data Register Empty |
| 23 | 0x002C | USART0_TX | USART0, Tx Complete |
| 24 | 0x002E | ANALOG_COMP | Analog Comparator |
| 25 | 0x0030 | ADC | ADC Conversion Complete |
| 26 | 0x0032 | EE_READY | EEPROM Ready |
| 27 | 0x0034 | TWI0 | TWI0 Transfer complete |
| 28 | 0x0036 | SPM_READY | Store Program Memory Ready |
| 29 | 0x0038 | USART1_RX | USART1 Rx Complete |
| 30 | 0x003A | USART1_UDRE | USART1, Data Register Empty |
| 31 | 0x003C | USART1_TX | USART0, Tx Complete |
| 32 | 0x003E | TIMER3_CAPT | Timer/Counter3 Capture Event |
| 33 | 0x0040 | TIMER3_COMPA | Timer/Counter3 Compare Match A |
| 34 | 0x0042 | TIMER3_COMPB | Timer/Coutner3 Compare Match B |
| 35 | 0x0044 | TIMER3_OVF | Timer/Counter3 Overflow |
| 36 | 0x0046 | USART0_START | USART0 Start Frame detection |
| 37 | 0x0048 | USART1_START | USART1 Start Frame detection |
| 38 | 0x004A | PCINT4 | Pin Change Interrupt 4 |
| 39 | 0x004C | CFD | Crystal Failure Detection |
| 40 | 0x004E | PTC_EOC | PTC End of Conversion |
| 41 | 0x0050 | PTC_WCOMP | PTC Window comparator mode |
| 42 | 0x0052 | SPI1_STC | SPI1 Serial Transfer Complete |
| 43 | 0x0054 | TWI1 | TWI1 Transfer complete |
| 44 | 0x0056 | TIMER4_CAPT | Timer/Counter4 Capture Event |
| 45 | 0x0058 | TIMER4_COMPA | Timer/Counter4 Compare Match A |
| 46 | 0x005A | TIMER4_COMPB | Timer/Coutner4 Compare Match B |
| 47 | 0x005C | TIMER4_OVF | Timer/Counter4 Overflow |
| 48 | 0x005E | USART2_RX | USART2 Rx Complete |
| 49 | 0x0060 | USART2_UDRE | USART2, Data Register Empty |
| 50 | 0x0062 | USART2_TX | USART2, Tx Complete |
| 51 | 0x0064 | USART2_START | USART2 Start Frame detection |
Note:
- When the BOOTRST Fuse is programmed, the device will jump to the Boot Loader address at reset, see Memory programming
- When the IVSEL bit in MCUCR is set, Interrupt Vectors will be moved to the start of the Boot Flash Section. The address of each Interrupt Vector will then be the address in this table added to the start address of the Boot Flash Section.
The table below shows reset and Interrupt Vectors placement for the various combinations of BOOTRST and IVSEL settings. If the program never enables an interrupt source, the Interrupt Vectors are not used, and regular program code can be placed at these locations. This is also the case if the Reset Vector is in the Application section while the Interrupt Vectors are in the Boot section or vice versa.
| BOOTRST | IVSEL | Reset Address | Interrupt Vectors Start Address |
|---|---|---|---|
| 1 | 0 | 0x0000 | 0x0002 |
| 1 | 1 | 0x0000 | Boot Reset Address + 0x0002 |
| 0 | 0 | Boot Reset Address | 0x0002 |
| 0 | 1 | Boot Reset Address | Boot Reset Address + 0x0002 |
Note: The Boot Reset Address is shown in Table Boot size configuration in Boot Loader
Parameters. For the BOOTRST Fuse “1” means unprogrammed while “0” means programmed.
When the BOOTRST Fuse is unprogrammed, the Boot section size set to 8K bytes
and the IVSEL bit in the MCUCR Register is set before any interrupts are enabled, the
most typical and general program setup for the Reset and Interrupt Vector Addresses
is:
Address Labels Code Comments 0x00000 RESET: ldi r16,high(RAMEND) ; Main program start 0x00001 out SPH,r16 ; Set Stack Pointer to top of RAM 0x00002 ldi r16,low(RAMEND) 0x00003 out SPL,r16 0x00004 sei ; Enable interrupts 0x00005 <instr> xxx ; .org 0x1F002 0x1F002 jmp EXT_INT0 ; IRQ0 Handler 0x1F004 jmp EXT_INT1 ; IRQ1 Handler ... ... ... ; 0x1FO36 jmp SPM_RDY ; SPM Ready Handler
When the BOOTRST Fuse is programmed and the Boot section size set to 8K
bytes, the most typical and general program setup for the Reset and Interrupt Vector
Addresses
is:
Address Labels Code Comments .org 0x0002 0x00002 jmp EXT_INT0 ; IRQ0 Handler 0x00004 jmp EXT_INT1 ; IRQ1 Handler ... ... ... ; 0x00036 jmp SPM_RDY ; SPM Ready Handler ; .org 0x1F000 0x1F000 RESET: ldi r16,high(RAMEND) ; Main program start 0x1F001 out SPH,r16 ; Set Stack Pointer to top of RAM 0x1F002 ldi r16,low(RAMEND) 0x1F003 out SPL,r16 0x1F004 sei ; Enable interrupts 0x1F005 <instr> xxx
When the BOOTRST Fuse is programmed, the Boot section size set to 8K bytes
and the IVSEL bit in the MCUCR Register is set before any interrupts are enabled, the
most typical and general program setup for the Reset and Interrupt Vector Addresses
is:
Address Labels Code Comments ; .org 0x1F000 0x1F000 jmp RESET ; Reset handler 0x1F002 jmp EXT_INT0 ; IRQ0 Handler 0x1F004 jmp EXT_INT1 ; IRQ1 Handler ... ... ... ; 0x1F036 jmp SPM_RDY ; SPM Ready Handler ; 0x1F03E RESET: ldi r16,high(RAMEND) ; Main program start 0x1F03F out SPH,r16 ; Set Stack Pointer to top of RAM 0x1F040 ldi r16,low(RAMEND) 0x1F041 out SPL,r16 0x1F042 sei ; Enable interrupts 0x1FO43 <instr> xxx