10.3 Low Frequency Crystal Oscillator

The Low-frequency Crystal Oscillator is optimized for use with a 32.768kHz watch crystal. When selecting crystals, load capacitance and crystal’s Equivalent Series Resistance (ESR) must be taken into consideration. Both values are specified by the crystal vendor. The oscillator is optimized for very low power consumption, and thus when selecting crystals, consider the Maximum ESR Recommendations:

Table 10-3. Maximum ESR Recommendation for 32.768kHz Crystal
Crystal CL [pF]Max. ESR [kΩ]
9.065
12.530

The Low-frequency Crystal Oscillator provides an internal load capacitance at each TOSC pin:

Table 10-4. Internal capacitance of Low-Frequency Oscillator
32kHz Osc. TypeInternal Pad Capacitance (XTAL1/TOSC1)Internal Pad Capacitance (XTAL2/TOSC2)
Ci of system oscillator (XTAL pins)6pF6pF
Ci of timer oscillator (TOSC pins)4pF4pF

The capacitance (Ce+Ci) needed at each XTAL/TOSC pin can be calculated by using:

Ce+Ci=2CL−Cs
where:
  • Ce - is optional external capacitors. (=C1, C2 as shown in Figure 10-2)
  • Ci - is the pin capacitance in Table 10-4.
  • CL - is the load capacitance for a 32.768kHz crystal specified by the crystal vendor.
  • CS - is the total stray capacitance for one TOSC pin.

Crystals specifying a load capacitance (CL) higher than 6pF require external capacitors applied according to above formula.

When this oscillator is selected, start-up times are determined by the SUT Fuses and CKSEL0 as shown in the following table.

Table 10-5. Start-up Times for the Low Frequency Crystal Oscillator Clock Selection
Power Conditions Start-up Time from Power-down and Power-saveAdditional Delay from Reset (VCC = 5.0V)CKSEL[0]SUT[1:0]
BOD enabled1K CK14CK(1)000
Fast rising power1K CK14CK + 4ms(1)001
Slowly rising power1K CK14CK + 65ms(1)010
Reserved011
BOD enabled32K CK14CK100
Fast rising power32K CK14CK + 4ms101
Slowly rising power32K CK14CK + 65ms110
Reserved111
Note:
  1. This option should only be used if frequency stability at start-up is not important for the application.