1.4 TCP/IP Berkeley UDP Relay
The Berkeley UDP Relay configuration demonstrates the use of multiple sockets for both sending and receiving. There are three different sub-functions of this application:
- UDP Relay, which accepts UDP packets on one socket, and sends the packets out on a different socket
- UDP Relay Client, which generates UDP traffic that is compatible with the UDP Relay Server
- UDP Relay Server, which receives and checks traffic for a packet count and reports is any packets are dropped
TCP/IP Berkeley UDP Relay MCC Configuration
The following Project Graph diagram shows the Harmony components included in the Berkeley UDP Relay demonstration application.
MCC is launched by selecting Tools > Embedded > MPLAB® Code Configurator from the MPLAB X IDE and after opening the project, TCP/IP demo project is ready to be configured and regenerated.
TCP/IP Root Layer Project Graph
The root layer project shows that SERCOM2 peripheral is selected to do read and write operation for TCP/IP commands.
This is the basic configuration with SYS_CONSOLE, SYS_DEBUG and SYS_COMMAND modules. These modules are required for TCP/IP command execution.

NOTE - The above screenshot contains FreeRTOS component and that is required for RTOS application. For bare-metal(non-RTOS) FreeRTOS component shouldn't be selected.
TCP/IP Configuration
- SAM E54 Xplained Pro

- SAM E54 Xplained Pro
TCP/IP Required Application
TCP/IP demo use these application module components for this demo.
Announce module to discover the Microchip devices within a local network.
Berkeley API module provides the Berkeley_Socket_Distribution (BSD) wrapper to the native Microchip TCP/IP Stack APIs. During this component selection, the required transport and network modules are also selected.
DHCP Client module to discover the IPv4 address from the nearest DHCP Server.
DNS Client provides DNS resolution capabilities to the stack.
TCP/IP Data Link Layer
Internal ethernet driver(gmac) is enabled with the external KSZ8091 PHY driver library. The MIIM Driver supports asynchronous read/write and scan operations for accessing the external PHY registers and notification when MIIM operations have completed.
TCP/IP Berkeley UDP Relay Hardware Configuration
This is the following section describes the hardware configuration used for this application demonstration.
- This section describes the required default hardware configuration use USB device as on board debugger and programmer for this application demonstration.
No hardware related configuration or jumper setting changes are necessary
Refer to the SAM E54 Xplained Pro User Guide

Connect the micro USB cable from the computer to the DEBUG USB connector on the SAM E54 Xplained Pro.
Establish a connection between the router/switch with the SAM E54 Xplained Pro through the RJ45 connector

TCP/IP Berkeley UDP Relay Running Application
This table list the name and location of the MPLAB X IDE project folder for the demonstration.
| Project Name | Target Device | Target Development Board | Description |
|---|---|---|---|
| sam_e54_xpro.X | ATSAME54P20A | SAM E54 Xplained Pro | Demonstrates the Berkeley UDP Relay on development board with ATSAME54P20A device and KSZ8091 PHY daughter board. This implementation is based on bare-metal(non-RTOS). |
| sam_e54_xpro_freertos.X | ATSAME54P20A | SAM E54 Xplained Pro | Demonstrates the Berkeley UDP Relay on development board with ATSAME54P20A device and KSZ8091 PHY daughter board. This implementation is based on FreeRTOS. |
There are several different commands available in the demonstration from the console port:
current - Displays the current configuration
start - Starts the packet relay service
stop - Stops the packet relay service
relayhost < host name > - Sets the host to which packets are to be relayed
relayport < port number > - Sets the port to which packets are to be relayed
ipv4port < port number > - Sets the IPv4 port that the relay server will listen to for packets to relay
ipv6port < port number > - Sets the IPv6 port that the relay server will listen to for packets to relay
relayclienthost < host name > - Sets the host to which packets are to be sent
relayclientiter < number > - The number of packets to generate
relayclientstart - Starts the relay client. This command must be used after the general application start. After a start is called, and the first packet is received by either the relay or the relay server, periodic updates will be sent to the console with information about the number of packets and bytes received.
Running Demonstration Steps
Build and download the demonstration project on the target board.
If the board has a SERCOM2 configuration:
A virtual COM port will be detected on the computer, when the USB cable is connected to USB-UART connector.
Open a standard terminal application on the computer (like Hyper-terminal or Tera Term) and configure the virtual COM port.
Set the serial baud rate to 115200 baud in the terminal application.
See that the initialization prints on the serial port terminal.
When the DHCP client is enabled in the demonstration, wait for the DHCP server to assign an IP address for the development board. This will be printed on the serial port terminal.
Alternatively: Use the Announce service or ping to get the IP address of the board.
Run tcpip_discoverer.jar to discover the IPv4 and IPv6 address for the board.
Execution:
After the successful board bring up, the console output becomes

To test the UDP packet relay with IPv4, send the following commands,
relayclienthost < ip address of the relay client >
relayclientiter < number of packets to relay >
relayhost < ip address of the host to which packets are to be relayed >
relayport < port number to which packets are to be relayed >
ipv4port < port number to which the relay server listens to, for packets to relay >
current
start
relayclientstart
Output - The above steps will relay the UDP packet from the host address set using the relayclienthost command to the destination address set by the command relayhost.
The relay packet will be received at the port set by command relayport.