1.7 TCP/IP SNMP NVM MPFS
The Microchip SNMP Server is a multi-lingual implementation, which supports SNMPv1, V2c, and V3 server features simultaneously. The SNMP Server is implemented to address the requirements of embedded applications and works with both IPv4 and IPv6 addresses.
TCP/IP SNMP NVM MPFS MCC Configuration
The following Project Graph diagram shows the Harmony components included in the SNMP NVM MPFS demonstration application.
MCC is launched by selecting Tools > Embedded > MPLAB® Code Configurator from the MPLAB X IDE and after opening the project, TCP/IP demo project is ready to be configured and regenerated.
TCP/IP Root Layer Project Graph
The root layer project shows that SERCOM2 peripheral is selected to do read and write operation for TCP/IP commands.
This is the basic configuration with SYS_CONSOLE, SYS_DEBUG and SYS_COMMAND modules. These modules are required for TCP/IP command execution.

NOTE - The above screenshot contains FreeRTOS component and that is required for RTOS application. For bare-metal(non-RTOS) FreeRTOS component shouldn't be selected.
The file system component is required to select MPFS module. This is the below snapshot for the FS configuration.

TCP/IP Configuration
- SAM E54 Xplained Pro

- SAM E54 Xplained Pro
TCP/IP Required Application
TCP/IP demo use these application module components for this demo.
Announce module to discover the Microchip devices within a local network.
DHCP Client module to discover the IPv4 address from the nearest DHCP Server.
DNS Client provides DNS resolution capabilities to the stack.
HTTPNET Server module is selected to run the web_server for the port number 80.
NBNS NetBIOS Name Service protocol associates host names with IP addresses. This assign of human-name host names to access boards on the same subnet.
SMTP CLIENT let applications send e-mails to any recipient worldwide.
SNTP Simple Network Time Protocol updates its internal time periodically using a pool of public global time servers.
SNMP and SNMPv3 are an application layer protocols that facilitates the exchange of management information among network devices.
Maximum SNMP Message Size can be increased and the value should be multiple of 32 bytes for larger GET-Bulk response.
TCP/IP Data Link Layer
Internal ethernet driver(gmac) is enabled with the external KSZ8091 PHY driver library. The MIIM Driver supports asynchronous read/write and scan operations for accessing the external PHY registers and notification when MIIM operations have completed.
TCP/IP SNMP NVM MPFS Hardware Configuration
This is the following section describes the hardware configuration used for this application demonstration.
- This section describes the required default hardware configuration use USB device as on board debugger and programmer for this application demonstration.
No hardware related configuration or jumper setting changes are necessary
Refer to the SAM E54 Xplained Pro User Guide

Connect the micro USB cable from the computer to the DEBUG USB connector on the SAM E54 Xplained Pro.
Establish a connection between the router/switch with the SAM E54 Xplained Pro through the RJ45 connector

TCP/IP SNMP NVM MPFS Running Application
The Non-Volatile Memory (NVM) Microchip Proprietary File System (MPFS) has the snmp.bib file along with other web page files stored in internal Flash and are accessed through the MPFS API.
This table list the name and location of the MPLAB X IDE project folder for the demonstration.
| Project Name | Target Device | Target Development Board | Description |
|---|---|---|---|
| sam_e54_xpro.X | ATSAME54P20A | SAM E54 Xplained Pro | Demonstrates the SNMP NVM MPFS on development board with ATSAME54P20A device and KSZ8091 PHY daughter board. This implementation is based on bare-metal(non-RTOS). |
| sam_e54_xpro_freertos.X | ATSAME54P20A | SAM E54 Xplained Pro | Demonstrates the SNMP NVM MPFS on development board with ATSAME54P20A device and KSZ8091 PHY daughter board. This implementation is based on FreeRTOS. |
Running Demonstration Steps
Build and download the demonstration project on the target board.
If the board has a SERCOM2 configuration:
A virtual COM port will be detected on the computer, when the USB cable is connected to USB-UART connector.
Open a standard terminal application on the computer (like Hyper-terminal or Tera Term) and configure the virtual COM port.
Set the serial baud rate to 115200 baud in the terminal application.
See that the initialization prints on the serial port terminal.
When the DHCP client is enabled in the demonstration, wait for the DHCP server to assign an IP address for the development board. This will be printed on the serial port terminal.
Alternatively: Use the Announce service or ping to get the IP address of the board.
Run tcpip_discoverer.jar to discover the IPv4 and IPv6 address for the board.
Execution :
After the successful board bring up, the console output becomes

The SNMP and SNMPv3 server is hosted by the application.
Open a SNMP manager (iREASONING SNMP manager is recommended) and Follow the steps given in iREASONING Networks MIB Browser section in the Third-Party help for complete details on using and configuring the application demonstration using the iREASONING SNMP Manager.
SNMP MIB Browser -
Several SNMP MIB browsers are available. Users can also install a customized MIB browser specific to their application.
Verify SNMP Get, GetNext, GetBulk, Set requests and Get response operations .
For SNMP v2c , the Agent can be configured with three Read communities (E.g - "public", "read", " ") and three Write communities (e.g - "private","write","public").
Community Index Read Write 1 public private 2 read write 3 ----- public Also the SNMP v2c Community string can be Configured from the web browser.

For SNMP v3, the Agent is configured as per the following table:
Type USER 1 USER 2 USER 3 USM User microchip SnmpAdmin root Security Level auth, priv auth, no priv no auth, no priv Auth Algorithm MD5 SHA1 N/A Auth Password < As Per The Configuration > < As Per The Configuration > N/A Privacy Algorithm AES N/A N/A Privacy Password < As Per The Configuration > N/A N/A The Microchip SNMP Stack supports both TRAP version 1 and TRAP version 2. The default trap output is a multi-varbind SNMPv3 TRAP version 2. Trap receiver setting of iReasoning to be selected and configured to visualize the trap output in the iReasoning MIB browser.