3.1 Driver Source Code Integration
To integrate Microchip WILC device driver's source code into the kernel's build system, perform the following steps:
- Add the driver source code, including the
Kconfigfile underlinux_root/drivers/net/wireless/microchip/wilc1000.Note: The WILCS02/ATWILC1000/ATWILC3000 all driver source code is located at the wilc1000 folder. - Edit
linux_root/drivers/net/wireless/Kconfigto add the path to the WILC's driver Kconfig sourcedrivers/net/wireless/mchp/Kconfig. - Edit
linux_root/drivers/net/wireless/Makefileto add the WILC's driver source codeobj-$(CONFIG_WLAN_VENDOR_MICROCHIP) += mchp/.