3.3 Kernel Configuration
The user must perform the following modifications in the Linux kernel configuration to enable Wi-Fi® support. The user must use the menuconfig to perform these modifications if the kernel is being built separately; otherwise, the user must add the corresponding CONFIG entries in the default defconfig file that buildroot is configured to use.
- Go to the directory of the Linux kernel and enter the following command:
Select the required configuration from the blue terminal to save and exit.$ make ARCH=arm menuconfig