18.1.4 Step 4: Select Frequency Mode
In the case where the noise is at (or close to) a frequency that is harmonically related to the sampling frequency then the noise issue becomes severe, as illustrated above. In this case, the oversampling frequency must be adjusted in order to avoid the noise.
This is particularly important in applications where a frequency sweep test is required, such as EN61000-4-6.
Acquisition Module (PTC)
| Available Frequencies (4 MHz PTC Clk) | |
|---|---|
| Frequency Selection | Frequency [kHz] |
FREQ_SEL_0 | 66.67 |
FREQ_SEL_1 | 62.5 |
FREQ_SEL_2 | 58.82 |
FREQ_SEL_3 | 55.56 |
FREQ_SEL_4 | 52.63 |
FREQ_SEL_5 | 50 |
FREQ_SEL_6 | 47.62 |
FREQ_SEL_7 | 45.45 |
FREQ_SEL_8 | 43.48 |
FREQ_SEL_9 | 41.67 |
FREQ_SEL_10 | 40 |
FREQ_SEL_11 | 38.46 |
FREQ_SEL_12 | 37.04 |
FREQ_SEL_13 | 35.71 |
FREQ_SEL_14 | 34.48 |
FREQ_SEL_15 | 33.33 |
FREQ_SEL_SPREAD | Variable frequencies |
- A single acquisition
frequency is selected, and oversampling takes place at this frequency only.
FREQ_SEL_0provides the fastest measurements andFREQ_SEL_15the slowest. If no high-performance EMC standards are required, but the application equipment generates noise, which interferes with a particular acquisition frequency, the designer may simply change the frequency. - A variable frequency is used
during oversampling. FREQ_SEL_SPREAD varies the frequency during the
acquisition oversampling. The delay is varied from 0 to 15 in a sawtooth
manner on successive samples during oversampling to apply a wider spectrum
of sampling frequency. Compared to single frequency acquisition, the
frequency spread option reduces the sensitivity to noise at a particular
‘worst-case’ frequency, but increases the range of noise frequencies around
that worst-case frequency which will show harmonic interference – albeit
with reduced severity of the noise effects. In many applications,
FREQ_SEL_SPREADis sufficient to achieve the required noise tolerance.
Frequency Hopping Module
Module ID: 0x0006
The frequency hopping module utilizes three or more base frequencies and a median filter to avoid using measurements taken with harmonic interference. The frequencies should be selected to minimize the set of crossover harmonics within the problem frequency band.
Each of the selected frequencies is used for acquisition oversampling during successive measurement cycles.
Frequency Hopping with 3 Frequencies:
- Cycle 1: All sensors measured with Frequency 0
- Cycle 2: All sensors measured with Frequency 1
- Cycle 3: All sensors measured with Frequency 2
- Cycle 4: All sensors measured with Frequency 0
- Cycle 5: All sensors measured with Frequency 1
Common Harmonics
No matter which frequencies are chosen, the possibility of noise at higher frequencies which are harmonics of more than one of the selected frequencies, exists.Further up the spectrum, there are frequencies which are harmonics of all available frequencies, but those superset harmonics are at higher frequencies and so are blocked by the low pass filter.
In some applications, the potential for exposure to noise frequencies may be an unknown and variable quantity.
For example, a device utilizing a USB charger may not always be plugged into the charger that it was supplied with. Inexpensive replacement chargers are often found to generate high levels of common-mode noise, and at variable frequencies – often in the same band as the acquisition frequencies.
A similar situation occurs with applications tested to EN61000-4-6 for conducted immunity. The test equipment sweeps through injected noise from 150 kHz to 80 MHz, in steps of 1%. This gives an excellent chance of hitting an interference frequency, which is a common harmonic of the HOP frequencies.
In both cases, no static selection of frequencies can ensure harmonic avoidance by the median filter.
Frequency Hopping with Auto-tune
Module ID: 0x0004
Frequency Hopping with auto-tune provides the cyclic frequency hopping with median filter functionality, extended to quantify the variance of signals as measured by each individual frequency.