7.2.1 Sensor Node Group
qtm_acquisition_control_t- A top-level container for an acquisition group
- Contains pointers to group and node memory containing configurations and run-time data
| Structure | Contents |
|---|---|
qtm_acquisition_control_t | qtm_acq_node_group_config_t
(*qtm_acq_node_group_config); |
qtm_acq_4p_saml10_config_t
(*qtm_acq_node_config); | |
qtm_acq_node_data_t
(*qtm_acq_node_data); |
qtm_acq_node_group_config_t- Common parameters, applied to all sensor nodes in the group
| Parameter | Size | Range/Options | Usage |
|---|---|---|---|
num_sensor_nodes | 16-bit | 4 to 65532 | The total number of sensor nodes configured in the group, for example, a number of 4P sets X4. |
acq_sensor_type | 8-bit | NODE_MUTUAL_4P | Parallel sets of 4 mutual capacitance sensor nodes. Each set contains 4x PTC X masks and 1x PTC Y masks for the measurement of XY capacitance. |
calib_option_select | 1 byte | Bits 3:0 Calibration type | Selects which parameter is auto-tuned for charge transfer. |
CAL_AUTO_TUNE_NONE | No auto-tune for charge transfer | ||
CAL_AUTO_TUNE_RSEL | Series resistor tuned to the largest value that allows full charge transfer | ||
CAL_AUTO_TUNE_PRSC | Prescaler tuned to the lowest (fastest) value that allows full charge transfer | ||
CAL_AUTO_TUNE_CSD | Charge share delay tuned to the lowest value that allows full charge transfer | ||
| Bits 7:4 Calibration target | Target charge time for sensor capacitance. | ||
CAL_CHRG_2TAU | Sensor charged for 2 x Time constant | ||
CAL_CHRG_3TAU | Sensor charged for 3 x Time constant | ||
CAL_CHRG_4TAU | Sensor charged for 4 x Time constant | ||
CAL_CHRG_5TAU | Sensor charged for 5 x Time constant | ||
freq_option_select | 1 byte |
to FREQ_SEL_15 | FREQ_SEL_0 to
FREQ_SEL_15 inserts a delay cycle between
measurements during oversampling, where 0 is the shortest delay, 15
the longest |
FREQ_SEL_SPREAD | FREQ_SEL_SPREAD varies this delay
from 0 to 15 in a sawtooth manner during the oversampling
set | ||
ptc_interrupt_priority | 1 byte | 1 to 3 | Arm® NVIC Interrupt priority |
wakeup_exp* | 1 byte | 0 to 15 | The Wake-up Exponent is the exponent for the power of two, representing the wake-up count in PTC core clocks |
|
Note: * - Not
available on all devices.
| |||
qtm_acq_saml10_node_config_t
| Parameter | Size | Range/Options | Usage |
|---|---|---|---|
node_xmask[4] |
4x4 bytes (16 bytes) 4x8* bytes (32 bytes) *AVR-DA | Array/bit field | Select X pin masks for NODE_MUTUAL_4P.Set the bit(s) at location(s) corresponding to X line number(s). For example: X0 only =0b00000001 = 0x01 X0 and X2 =
0b00000101 = 0x05 |
node_ymask |
4 bytes 8* bytes *AVR-DA |
(bit field) |
Select Y pin mask. Set the bit(s) at location(s) corresponding to Y line number(s). For example: Y5 only = Y1, Y2 and Y7 = |
node_csd | 1 byte |
For SAM L1x: 0 to 255 For ATtiny81x,161x,321x: 0 to 31 |
The number of delay cycles to ensure the charging of the sensor node capacitances Note: If auto-tune is
enabled, this value is used for initial compensation capacitor
calibration. Ensure it allows sufficient time to charge the
sensor.
|
node_rsel_prsc | 1 byte |
Bits 7:4 = RSEL
|
Internal Y line series resistor selection * May not be available for all devices AVR-DA: 70 kΩ, 80 kΩ, 120 kΩ, 200 kΩ |
|
Bits 3:0 = PRSC
|
Clock Prescaler Acquisition clock is derived and scaled from CPU clock for AVR® devices. * May not be available for all devices. AVR-DA: 6 , 12, 14 ** **The numbers correspond to the prescaler value. | ||
node_gain | 1 byte |
Bits 7:4 = Analog Gain
|
Analog Gain Setting Integration capacitor adjusted to control integrator gain. |
| Bits 3:0 = Digital Gain
| Digital Gain Setting The accumulated sum is scaled to Digital Gain. | ||
node_oversampling | 1 byte |
|
The number of samples to accumulate for each measurement. Note: Oversampling must
be configured to be greater than or equal to Digital Gain for
correct operation.
|
qtm_acq_node_data_t- Individual node run-time data (array)
| Parameter | Size | Range/Options | Usage |
|---|---|---|---|
node_acq_status | 1 byte | Bit 7 |
The sensor node capacitance exceeds the maximum compensation capacitance supported. |
| Bit 6 | 1 = Charge transfer tuning complete | ||
| Bit 5 | 1 = Calibration state set | ||
|
Bit 4: Bit 2 (3 Bits) Node calibration state
| Indicates whether calibration is ongoing and its current stage | ||
|
Bit 1: Calibration Request |
Write a ‘ (Reset to ‘ | ||
|
Bit 0: Enabled |
Write a ‘ | ||
node_acq_signals | 2 bytes | Most recent measurement for this sensor node. | This is a 16-bit unsigned value. Accumulated and scaled as per
|
node_comp_caps | 2 bytes | Hardware calibration data | Indicates tuning of the compensation circuit for this node |