2.1.1 CCC Location
You must choose a physical location for the CCC pair:
- CCC_NW
- CCC_NE
- CCC_SW
- CCC_SE
The package pin names for the selected location are displayed next to the dedicated pads in the Advanced tab of each CCC. It is important to ensure that the dedicated input pad selected in the configurator GUI matches the board-level clock input pin assignment.