24.6.2 Sending Frames with 9 Data Bits
If 9-bit characters are used (UCSZ = 7), the ninth bit must be written to the TXB8 bit in UCSRB before the Low byte of the character is written to UDR. The following code examples show a transmit function that handles 9-bit characters. For the assembly code, the data to be sent is assumed to be stored in registers R17:R16.
Assembly Code Example(1)
USART_Transmit: ; Wait for empty transmit buffer sbis UCSRA,UDRE rjmp USART_Transmit ; Copy 9th bit from r17 to TXB8 cbi UCSRB,TXB8 sbrc r17,0 sbi UCSRB,TXB8 ; Put LSB data (r16) into buffer, sends the data out UDR,r16 ret
void USART_Transmit( unsigned int data ) { /* Wait for empty transmit buffer */ while ( !( UCSRA & (1<<UDRE))) ) ; /* Copy 9th bit to TXB8 */ UCSRB &= ~(1<<TXB8); if ( data & 0x0100 ) UCSRB |= (1<<TXB8); /* Put data into buffer, sends the data */ UDR = data; }
Note: 1. These transmit functions are
written to be general functions. They can be optimized if the contents of the UCSRB is
static. For example, only the TXB8 bit of the UCSRB Register is used after
initialization.
The ninth bit can be used for indicating an address frame when using multi processor communication mode or for other protocol handling as for example synchronization.