1.2.6.6 WDRV_PIC32MZW_AssocPeerAddressGet Function
WDRV_PIC32MZW_STATUS WDRV_PIC32MZW_AssocPeerAddressGet (
WDRV_PIC32MZW_ASSOC_HANDLE assocHandle, WDRV_PIC32MZW_MAC_ADDR *const pPeerAddress
)
C
Summary
Retrieve the current association peer device network address.
Description
Attempts to retrieve the network address of the peer device in the current association.
Precondition
WDRV_PIC32MZW_Initialize should have been called. WDRV_PIC32MZW_Open should have been called to obtain a valid handle. A peer device needs to be connected and associated.
Parameters
Param | Description |
assocHandle | Association handle. |
pPeerAddress | Pointer to structure to receive the network address. |
Returns
WDRV_PIC32MZW_STATUS_OK - pPeerAddress will contain the network address.
WDRV_PIC32MZW_STATUS_NOT_OPEN - The driver instance is not open.
WDRV_PIC32MZW_STATUS_INVALID_ARG - The parameters were incorrect.
WDRV_PIC32MZW_STATUS_REQUEST_ERROR - The request to the PIC32MZW was rejected or there is no current association. WDRV_PIC32MZW_STATUS_RETRY_REQUEST - The network address is not
available but it will be requested from the PIC32MZW. WDRV_PIC32MZW_STATUS_NOT_CONNECTED - Not currently connected.
Remarks
If the network address is not currently known to the driver (stored within the PIC32MZW) a request will be sent to the PIC32MZW and the return status will be WDRV_PIC32MZW_STATUS_RETRY_REQUEST.