2.9.3.3 Single-Step Verification
There are two versions of the bootstrap image format. One format is for the tagged version, AES-CMAC, which is used for authenticity. The other version is for the DSS version, when a digital signature is used.
For both versions, the header authenticity is checked with an AES-CMAC, and random data are used to pad the header.
The following figure shows a tagged bootstrap image format.
Auth.Data value is as follows:| Mode | RFU | Security Data Size |
0x02 or 0x03 | 0x00 | 0x0010 |
Mode is encrypted, tagged. There is no additional data for this mode.
When DSS mode is used, the image format is shown in the figure below.
The Auth.Data field is as follows:
| Mode | RFU | Additional Data Size |
0x04,0x05 | 0x00 | 0xyyyy |
Mode is encrypted, signed with a DSS. A security blob is added following the bootstrap
image; Security data size specifies the size in bytes of this security
blob used to certify the image.