38.5.3.10 Initialization
The following steps are required to configure the ADC for operation:
- Configure input pins for operation as analog input pins, ADC_AINk.
- Configure a GCLK generator to provide the GCLK_ADC clock (PCHCTRLm index = 33).
- Configure ADC registers:
- Copy factory-provided calibration values from the CAL OTP Register FCCFG65 into CALCTRL for all the ADC in use by the application.
- Configure CTRLA as needed but do not set CTRLA.ENABLE.
- Configure CTRLD, choosing the clock divider (CTLCKDIV) for the CTL_CLK clock based on the GCLK_ADC, Voltage Reference (VREFSEL), and Wake-up Delay Exponent (WKUPEXP).
- (Optionally) Enable ADC interrupts for FIFO support using CTLINTENSET. Optionally enable the interrupts for VREFRDY and Core n ready. (Or these conditions can be monitored by watching CTLINTFLAG in a while(1) loop.) Enable interrupt vector 132 (ADC Global Interrupt) in the NVIC.
- Enable ADC interrupts using the INTENSET registers. Enable the corresponding NVIC interrupt vector 133.
- For each ADCn, configure its Control register CORCTRLn:
- Set the clock divider, ADCDIV, for the ADC Module clock, CORE_CLK[n].
- Set the sample count SAMC (ADCDIV and SAMC determine the ADC Module’s sample rate fs).
- If ADC resolution other than 12 bits is desired, set it using SELRES.
- Other settings in CORCTRLn as needed.
- Setup differential channels using CHNCFG3n.DIFFk = 1 for signals pairs k and k+1 (k even).
- Select the input channels for each scan using CHNCFG2n.CSSk = 1.
- Set the data format for each sample using CHNCFG2n.FRACTk and CHNCFG3n.SIGNk.
- Setup channel triggers.
- (Optional: Setup up the Digital Filter and Digital Comparator associated with each of the four modules).
- Enable the ADC by setting CTRLA.ENABLE = 1.
- Wait until CTLINTFLAG.VREFRDY = 1, either using an ISR or polling in a while(1) loop. This signals that the chip’s analog environment is ready.
- Wait for CRRDYn to go high in CTLINTFLAG, indicating that the corresponding ADC Module is ready. This can be polled in a while(1) loop or trapped by the ISR attached to the ADC Global Interrupt.