26.4.3.1.3 Adding a Descriptor Between Existing Descriptors
To insert a new descriptor 'C' between two existing descriptors ('A' and 'B'), the descriptor currently executed by the DMA must be identified.
- If DMA is executing descriptor B, descriptor C cannot be inserted.
- If DMA has not started to execute
descriptor A, follow these steps:
- Set the descriptor A VALID bit to
'
0'. - Set the DESCADDR value of descriptor A to point to descriptor C instead of descriptor B.
- Set the DESCADDR value of descriptor C to point to descriptor B.
- Set the descriptor A VALID bit to
'
1'.
- Set the descriptor A VALID bit to
'
- If DMA is executing descriptor A:
- Apply the software suspend command to the channel.
- Perform Step 2.1 through Step 2.4.
- Apply the software resume command to the channel.