1.3.3.12 PAL_DataIndication Typedef
C
typedef void (*PAL_DataIndication)(uint8_t *pData, uint16_t length);
Summary
Pointer to a PAL Data Indication event handler function.
Description
This data type defines the required function signature for the PAL reception data indication event handling callback function. When PAL_Init is called, a client must register a pointer whose function signature (parameter and return value types) matches the types specified by this function pointer in order to receive transfer related event calls back from the PAL.
Parameters
| Param | Description |
|---|---|
|
pData |
Pointer to the data buffer containing received data |
|
length |
Length of the received data in bytes |
Returns
None.
Example
static void _plcDataIndication(uint8_t *pData, uint16_t length)
{
}
PAL_INIT palInitData;
palInitData.palHandlers.palDataIndication = _plcDataIndication;
palInitData.palHandlers.palTxConfirm = _plcTxConfirm;
palInitData.palHandlers.palRxParamsIndication = _plcRxParamsIndication;
PAL_Init(&palInitData);
Remarks
None.